Industry Online Support
Technical Forum
1/2/2013 7:00 PM | |
Joined: 9/27/2006 Last visit: 4/19/2024 Posts: 12256 Rating: (2664) |
Hello SMS; The Sitopbuffer module accumulates energy to hold up a Sitop power supply fora short period of time in case of an interruption of AC input current. Not quite a UPS, but also not the same price range: SITOP buffer module Description The optional mains buffer module is a built-in device belonging to the SITOP series. The device must be installed taking into account all relevant DIN/VDE specifications and other national standards. It is used in combination with a stabilized 24 V load power supply unit of the SITOP serie to buffer the load current if the AC power supply is interrupted temporarily. Buffering time : -with 40 A load current: 200 ms -with 20 A load current: 400 ms -with 10 A load current: 800 ms -with 5 A load current: 1.6 s
|
Last edited by: dchartier at: 1/2/2013 7:01 PM |
|
Follow us on