(5)| 2/4/2017 5:32 PM | |
|
Joined: 9/23/2005 Last visit: 12/14/2025 Posts: 4429 Rating:
|
“Simple Samples” are small projects that demonstrate simple features. The target is give a quick overview about the theme and be used as start point for related discussions. Follow there are a short description and the configuration main steps. Description: One of news of TIA V14 is the possibility todefine arrays with no pre defined size as block parameter (Array(*) as new parameter data type). New instructions (LOWER_BOUND, UPPER_BOUND are available to determining the array boundaries. This make be possible to build general proposes block that automatically adapts by itself by usage. Benefits
This sample program shows a block (Block_1) that calculate the average value of a array of data: Tips:
Requirements: TIA V14. Project: Archived program, compressed (zip) AttachmentProject2.zip (1637 Downloads) |
Last edited by: Denilson Pegaia at: 2/4/2017 5:33:21 PMDenilson Pegaia |
|
This contribution was helpful to
|
|
| 7/25/2017 8:24 AM | |
|
Posts: 8171 Rating:
|
New question published by guileser is split to a separate thread with the subject Can "Array[*]" be used on a S7-1200 CPU?. Best regards |
Follow us on