4/26/2016 10:55 AM | |
Joined: 8/25/2006 Last visit: 4/17/2024 Posts: 2203 Rating: (277) |
Hello. May be with some modifications it is possible. |
4/26/2016 10:56 AM | |
Posts: 107 Rating: (20) |
No, it's not possible to install STEP7 V5.5 SP4 on Windows Server 2012 You can use Siemens Compatibility tool for reference |
Last edited by: Mohamed Ali at: 4/26/2016 10:59:56 AM |
|
4/26/2016 11:03 AM | |
Joined: 7/22/2008 Last visit: 4/14/2022 Posts: 1884 Rating: (174) |
RIP |
Last edited by: 1test at: 6/8/2016 9:29:21 AM~(‾▿‾)~ |
|
4/26/2016 3:39 PM | |
Joined: 9/7/2007 Last visit: 8/30/2023 Posts: 550 Rating: (61) |
High Alex Wai Good news As of yesterday Siemens had issued the new Operating systems compatibilities for STEP 7 (STEP 7 Professional) which indicates that Step 7 SP4 Upd9 (2010 SR4) is compatible with Microsoft Windows Server 2012 R2 Standard Edition (64-Bit) This was a part of PCS7 8.2 Compatibility List that was issued 25-4-2016 I think this will be updated in Step 7 soon
AttachmentPCS-7_V8.2_compatibility-list_en_2016-04-25.xlsx (357 Downloads) |
Best Regards |
|
This contribution was helpful to2 thankful Users |
4/27/2016 6:38 AM | |
Joined: 5/12/2006 Last visit: 4/18/2024 Posts: 22207 Rating: (2979) |
Not really good news The HF9 need a installed Step7 V5.5 SP4! And V5.5 SP4 can't installed on Windows Server 2012! |
This contribution was helpful to1 thankful Users |
4/27/2016 6:43 AM | |
Joined: 3/26/2015 Last visit: 3/1/2024 Posts: 7 Rating: (0) |
Hi Duris, The story is I need to make a pair of WinCC Redundant Server. At the beginning, the following software are designed to use: - WinCC v7.2, Step7 v5.5, Windows Server 2008 As requesting by my customer, Microsoft will not support Win Server 2008 shortly. Therefore, I need to change to Windows Server 2012. Unfortunately, WinCC V7.2 does not support Win Server 2012. I changed the software as below: - WinCC V7.3, Step7 v5.5, Windows Server 2012 I asked siemens support and the reply is Step v5.5 is not tested on other OS which listed out in the readme.rtf. Use on other OS at my own risk.
|
This contribution was helpful to1 thankful Users |
4/27/2016 6:46 AM | |
Joined: 3/26/2015 Last visit: 3/1/2024 Posts: 7 Rating: (0) |
Any new STEP7 v5.5 SP4 incl. Upd9 software can be order ? It is a quite stupid update for compatiable to new OS.
|
Follow us on