10/19/2021 11:50 AM | |
Joined: 2/7/2020 Last visit: 4/23/2024 Posts: 4 Rating:
|
Good day! System Description: There is a PLC 1200 and a CP-1242-7 GPRS module. TeleControl Server Basic V3.1 + HF1 is installed on the remote station, I need to visualize the data from the PLC using WinCC Advanced. The problem is that I cannot see the PLC data in the OPC server using UaExpert. Help me please. Screenshots of settings in the attachment (you need to remove the * .txt extension and unzip the archive with the photo).
AttachmentFoto.rar.txt (69 Downloads) |
Last edited by: Serega0629 at: 10/19/2021 11:52:22 |
|
10/19/2021 1:27 PM | |
Joined: 4/25/2017 Last visit: 7/29/2024 Posts: 427 Rating:
|
Hi, Do you know this application examples? Inter-Station Communication between S7-1200 Stations Using TCSB V3.1 via CP 1242-7 V2 |
Best Regards, |
|
10/21/2021 1:37 PM | |
Joined: 2/7/2020 Last visit: 4/23/2024 Posts: 4 Rating:
|
Good afternoon. |
Follow us on