5/12/2012 8:00 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
Hello, Hereby I am attaching Technical Specification for UL Redundancy Module which can be directly used with two no. of SM321 digital input module. Hope it helps.
AttachmentUL16DIOR-CC-TB..pdf (203 Downloads) |
VANDE MATARAM..... |
|
5/12/2012 8:04 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
Technical Specification for UL Redundancy Module which can be directly used with two no. of SM322 digital input module.
AttachmentUL16DOREDD25OFI-TB FOR 6ES7322-1BL00-0AA0..pdf (86 Downloads) |
VANDE MATARAM..... |
|
5/12/2012 8:16 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
Technical Specification for UL Redundancy Module which can be directly used with two no. of SM331 analog input module.
AttachmentUL08AI(RED)-D25 SPD FOR 6ES7331-7KF02-0AB0.pdf (153 Downloads) |
VANDE MATARAM..... |
|
This contribution was helpful to
2 thankful Users |
5/12/2012 10:35 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
Technical data for UL Module to connect two no. Of SM332 analog output module. |
VANDE MATARAM..... |
|
5/12/2012 10:37 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
Technical data for UL Module to connect two no. Of SM332 analog output module.Technical data for UL Module to connect two no. Of SM332 analog output module.
AttachmentUL08AO(RED)-SRC-D25_I FOR 6ES7332-5HF00-0AB0.pdf (160 Downloads) |
VANDE MATARAM..... |
|
5/12/2012 11:53 AM | |
Joined: 3/18/2008 Last visit: 7/28/2020 Posts: 1750 Rating:
|
More information for connection with DI Module. AttachmentUL16DIFRED-D25 FOR 6ES7321-7BH01-0AB0.pdf (75 Downloads) |
VANDE MATARAM..... |
|
This contribution was helpful to
1 thankful Users |
5/16/2014 8:06 AM | |
Posts: 347 Rating:
|
new question is splittet to Quote for UL modules |
This contribution was helpful to
1 thankful Users |
Follow us on