10/30/2014 12:28 PM | |
Posts: 567 Rating: (106) |
Hi, please check if user name and pass word are the same on both PC stations. If OS is not in the same subnet check if you have configured a multicast proxy in the settings of the SIMATIC Shell. Please check if the network adapter which is used for the terminal bus on fist place in the advanced network settings (windows). You can also find some more points to check under the following link: http://support.automation.siemens.com/WW/view/en/33123686 |
10/30/2014 2:12 PM | |
Posts: 567 Rating: (106) |
Hi, the network settings should be configured as descripted in PCS 7 compendium part a (chapter 3.3.6) http://support.automation.siemens.com/WW/view/en/63187279 Isthe os server the same subnet? If not than you have to add multicast proxy in the SIMATIC Shell. To get more information about the multicast proxy press the help button in SIMATIC Shell. |
6/28/2020 5:18 PM | |
Joined: 9/9/2015 Last visit: 8/5/2024 Posts: 727 Rating: (277) |
Dear travis128154, Please follow my step here to check your system 1. Ping check using computer name from ES to OS and OS to ES, eg. Ping computername If this failed, please check your host file. Run this command "nbtstat -c" , ensure all the entry are correct. 2. win+r -> lusrmgr.msc , ->User -> look for your device specific account (window logon account) -> right click-> member role-> ensure "SIMATIC HMI" is there for OS Server and OS Client and ensure "SIMATIC NET" in OS Server For ES, ensure SIMATIC NET, SIMATIC HMI, Siemens TIA Engineer in the ES Windows Logon group. 3. Check the Target OS path folder -> at the local station-> ensure the project folder is shared and permission is given -> right click at the folder-> properties-> sharing -> tick the sharing -> add the SIMATIC HMI into the folder permission. And next tab -> Security -> add SIMATIC HMI -> tick read/write access. 4. check OS Server Station configuration. ensure the station configuration is healthy. If step 1-3 cannot help, I will continue to explain the station config. Hope this is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on