3/13/2020 2:49 PM | |
Posts: 9 Rating: (0) |
Hello All, I installed TIA Portal V14 to my new pc. It is lisenced. Simulation is okey. However when ı upload to the program. I can not use monitoring on /off function. I searched the solution in forum. I changed the pc tiime and set time ( take from PG/PC) But it is not work. Also ı download the program after uploading. I removed the TIA portal program then install again. Today ı upgraded the TIA/winCC program. All is not work I noticed that MPI adaptör MPI led is flashing so fast. That's mean if monitoring on/ off icon will usable my problem will be solved. Kind Regards, AttachmentSiemens_Forum.docx (70 Downloads) |
This contribution was helpful to1 thankful Users |
3/13/2020 3:47 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello, Are you using latest Service Packs and Updates? Best regards, Wizard |
3/13/2020 3:53 PM | |
Posts: 9 Rating: (0) |
Hello Wizard, I am using V14 SP1 and update 9. My pc have connection with PLC just monitoring on/off icon is disable. Kind Regards, Musa UÇAN |
3/13/2020 4:37 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Hello, Have you seen this link: How do you uninstall STEP 7 (TIA Portal) completely? What is the version of Windows, you are using? Best regards, Wizard |
3/13/2020 6:05 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating: (24) |
Hello, musaucan, When you said you uploaded the program to your PG/PC from a CPU, Do you know the program available on the CPU online downloaded using the same version of the TIA portal that you are having installed On your PC right now? It could be version or special batch missing related issues. By the way, please refer to this post, it may be helpful to you. |
Last edited by: Maruthakasi_S at: 03/13/2020 18:11:02Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
3/13/2020 6:50 PM | |
Posts: 9 Rating: (0) |
Wizard, Windows 10 i am using |
3/13/2020 6:58 PM | |
Posts: 9 Rating: (0) |
Hello Maruthakasi_S, I am using MPI cable to connect to plc. Not TCP/IP |
Follow us on