3/11/2019 6:16 PM | |
Posts: 16 Rating: (0) |
Hello everyone, Is it possible that TIA portal v15.1 (S7-1200) is not compatible with this modules: - CPU 1214C DC/DC/DC 6ES7 214-1AG40-0XB0 v4.2 (also v4.1 and v4.0), - Communication processor CP1242-7 GPRS V2 v3.0 (or v3.1), - Analog I/O module SM1234 6ES7 234-4HE32-0XB0 v2.0? I've seen that in Siemens Compatibility Tool. When I use TIA portal v15 everything is OK. With TIA portal v15.1 I can't connect to the PLC. If this is the case, what is my solution for using TIA portal v15.1 with those modules? Would there be any new update for v15.1 that will enable that? Thanks. |
Follow us on