11/25/2021 2:59 PM | |
Joined: 3/11/2019 Last visit: 5/8/2024 Posts: 1408 Rating: (254) |
Hi as Rafal already mentioned, you need to install STEP 7 Safety in order to use safety functions in the project. The download can be found with following link. After the trial period also a license is needed. If only cpu-1200 are used, the basic version is enough. SIMATIC STEP 7 Safety Advanced V15 – TRIAL
regards sancurz |
Feedback appreciated, please rate |
|
This contribution was helpful to2 thankful Users |
12/27/2021 12:56 PM | |
Joined: 5/29/2019 Last visit: 4/16/2024 Posts: 10 Rating: (0) |
OK, thanks everybody for the help. So if I am trying to configure a 1214 FC PLC with the components I mentioned above I only need the Basic License?
|
Follow us on