6/7/2021 8:31 AM | |
Joined: 9/6/2014 Last visit: 5/1/2024 Posts: 209 Rating: (6) |
HI IF I use new version (tia 17) T is that support lower version or not ? |
6/7/2021 8:42 AM | |
Joined: 12/18/2014 Last visit: 5/15/2024 Posts: 33037 Rating: (4082) |
Delivery Release SIMATIC STEP 7 Professional / Basic V17Compatibility with other products STEP 7 V17 can be installed on a PC in parallel with other versions of STEP 7 V13 SP2 to V16, STEP 7 V5.6 or higher. You can find additional information on compatibility in the FAQ "Compatibility tool for automation and drive technology" > 64847781 Projects as from TIA Portal project version V13 SP1 can be upgraded directly to V17. Upgrading from previous project versions (V11 ... V13) is carried out on the basis of the TIA Portal products (for example STEP 7) used in the project in version V13 SP1 or V13 SP2 (most recent update recommended). |
This contribution was helpful to2 thankful Users |
6/7/2021 3:27 PM | |
Joined: 9/6/2014 Last visit: 5/1/2024 Posts: 209 Rating: (6) |
THANK YOU. Really , variety of TIA was big problem for me and now I can relax and I take simply breathing ! Bless you |
9/27/2021 9:22 AM | |
Joined: 6/19/2017 Last visit: 5/15/2024 Posts: 8062 Rating: (164) |
New question published by RHD1969 is split to a separate thread with the subject Make Upload of program in TIA portal V13, but TIA portal is V17. Best regards |
My Forum is the place to personalize your profile, |
|
Follow us on