12/20/2016 9:32 AM | |
Joined: 8/3/2009 Last visit: 4/17/2024 Posts: 12790 Rating: (1632) |
Hello Jan Yes Connection with Wireless Lan ist always tricky because the WLAN Access points often do not forward the MAC Adress Broadcast Telegrams of the "accessable devices or something else" often you can only use a direct IP Connetion if the Access Point has no such Option to set. you say teh Ping to the Device you want to load or go online is OK and you can do also a Online Sight. At the Panel just look if the Transfer settings is Ethernet not PN/IE and in the Transfer Option in TIA Portal also use Ethernet (or PN/IE on both side) look to this FAQ: https://support.industry.siemens.com/cs/ww/en/view/88633853 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on