Industry Online Support
Technical Forum
2/25/2012 6:00 PM | |
Joined: 6/4/2008 Last visit: 9/15/2024 Posts: 1497 Rating: (324)
|
A 19mm bolt is massive, what the heck are you fixing the inverter to, a Chieftan tank? Is 19mm the bolt shaft dimensions, or the AF size of the socket you are using to tighten with? I suspect you are using a 19mm socket in which case the bolt thread itself will be an M12 or M14. What Inverter are you using? What is the nut/bolt 's function (Blind hole, clamping cable tag to copper busbar etc)? What is the nut & bolt manufactured from Nn plated steel,ST/ST, or nylon?
AttachmentPages from MC_BA_Einbau_AC_d_e.pdf (157 Downloads) |
Last edited by: Graeme at: 2/26/2012 2:42 PMAttachment!! |
|
Follow us on