Industry Online Support
Technical Forum
12/15/2008 8:45 AM | |
Joined: 5/28/2008 Last visit: 12/8/2015 Posts: 901 Rating:
|
Hello gabriel74, maybe this will help you: http://support.automation.siemens.com/WW/view/de/19701610 This only is helpful, if the Image on the OS PC is newer, then the Operating system on the TP177 A. If not: then you have 2 possibilities: 1. take a newer winCC flexible version to project 2. downgrade the TP 177 A firmware to an older one I hope, i could help you... regards manfred HO Ho Ho |
Follow us on