4/27/2010 5:07 PM | |
Joined: 2/5/2009 Last visit: 7/4/2024 Posts: 36 Rating: (1) |
Is possible you explain me better, you say how many memory i need in tha card? |
4/28/2010 12:19 PM | |
Joined: 2/5/2009 Last visit: 7/4/2024 Posts: 36 Rating: (1) |
Hi, |
4/28/2010 1:48 PM | |
Joined: 4/24/2006 Last visit: 9/20/2024 Posts: 8742 Rating: (1168)
|
Hi, I would suggest the following: Perform an OS update, with the option 'Reset to factory settings', see the following link: how do you do an operating system update (OS update) on operator panels? Then when you download the project, have a look at Control panel -> OP and look how much memory is occupied. (If I remember well, you can shift, to free some memory for project) Best regards, Wizard |
Follow us on