6/3/2014 10:58 PM | |
Posts: 5 Rating:
|
Dear Sir, Thank you very much for your respond. This both panels are TP177B so the type is same. Do you think it is possible?
|
6/3/2014 11:06 PM | |
Posts: 5 Rating:
|
Dear Sir, Thank you for your reply. please check that both part numbers are for TP177B so what is your idea regaring this.
|
6/5/2014 5:11 PM | |
Joined: 1/21/2013 Last visit: 6/6/2024 Posts: 4620 Rating:
|
Hello swasthika, Should be possible, have a look this thread: Replacement of the siemens Panel |
This contribution was helpful to
2 thankful Users |
6/5/2014 7:08 PM | |
Joined: 5/28/2008 Last visit: 7/30/2024 Posts: 4514 Rating:
|
Hello, A short answer; It will work without problems. When you create a WinCC flexible project for TP177B, you select the panel type and you don't select its part number. So, after compile the compiled file of your project can be downloaded to any TP177B. Both mentioned panels are of the same type. Not the same part number. So, the compiled file which contains a project suitable for a TP177B can be downloaded to TP177B. Thus why it will be possible to use both panels. More over as per thislink, Siemens tells that "6AV6642-0BC01-1AX1" is sucessor of "6AV6642-0BC01-1AX0". And the same issue was discussed in the following thread. Please revise my post in this thread. Hope this helps.
|
Ayman Elotaify |
|
This contribution was helpful to
3 thankful Users |
Follow us on