10/7/2010 9:20 AM | |
Joined: 4/24/2006 Last visit: 4/25/2024 Posts: 8613 Rating: (1147) |
Dear Wubbo, Here is link to manual: TP27, TP37 Touch panels perhaps chapter. 12.2.3 might help. Rebooting of panel, can because of communication problems. Best regards, Wizard |
10/12/2010 7:45 PM | |
Joined: 9/27/2006 Last visit: 4/25/2024 Posts: 12257 Rating: (2665) |
Hello Wubbo; Based on the two following articles,2 TP27 can easily be connected to a single S7-CPU: Max number of operator panels on a CPU:/tf/WW/en/Posts/30406Max. number of CPUs connected to an operator panel: http://support.automation.siemens.com/WW/view/en/15363798 |
Follow us on