10/11/2017 10:27 AM | |
Posts: 34 Rating: (0) |
Hi I had two engineering station (preconfigured and licensed), I will use only one ES and I want to make the second an OS Client. Do I need any additional Licenses to do it ? ------------------------------------------------------------------------------------------ |
Last edited by: Amen Allah at: 10/11/2017 10:32:27 AMLast edited by: Jen_Moderator at: 10/11/2017 12:52:58 PMNew subject after splitting Last edited by: Amen Allah at: 10/11/2017 1:08:41 PM |
|
10/11/2017 3:42 PM | |
Joined: 3/14/2008 Last visit: 5/7/2024 Posts: 2066 Rating: (928)
|
Hi, Yes, you need additional licenses in order to use the ES as OS client. You will need at least the following license: - 1x OS client (6ES7658-2CX28-0YB5) In case you use additional addons or tools like SFC's, you will need a license for that as well (basically the same as you have for your other OS clients): - 1x SFC Visualization (6ES7652-0XD28-2YB5) Take a look at the following document: PCS7 V8.2 Standard Architectures It will show you a lot of PCS7 configurations. On page 32 is an example for using ES as OS client. You also need to adapt the PCS7 project as well-> Inserting an OS application client for the ES PC station, configuring and downloading etc..
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on