8/30/2016 10:47 AM | |
Posts: 4 Rating: (0) |
dear all i have a problem with a machine that is fitted with s7 315 cpu and a simotion c230-2 system for some reason suddenly the mmc on the simotion lost its program and i got a new mmc but i was not able to open the program with my current scout v2.0 i tried to use scout v4.3 also couldnt open the program i know that the program is written using a very old scout version but i dont understant why i can not convert it using newer versions i am attaching the program here so please guys if any one could open it tell me what was the scout version that he used thanks joe AttachmentEla14_09_04.zip (130 Downloads) |
8/30/2016 12:12 PM | |
Joined: 10/11/2006 Last visit: 9/18/2024 Posts: 5906 Rating: (804)
|
following your enquiry, we trie to open the project with Scout 3.2. We see the source code of units but no Hardware C3230-2 was generated in Attached PDF document I copy some screens from decompile. The best way should be to get the project as an XML-Export V3.1 .for the upgrade.
AttachmentOpening the project with Scout 3.pdf (177 Downloads) |
With best regards, |
|
Follow us on