(1)| 10/23/2017 4:37 PM | |
|
Posts: 2 Rating:
|
Good Afternoon All, I have ran into a few problems trying to set up communications between an Allen Bradley Control Logix and a S7-1200. I saw this post: https://support.industry.siemens.com/cs/document/108740380/open-user-communication-to-3rd-party-control-system-(clx-glx-controller)?dti=0&lc=en-WW Hoping that it could be a simple solution, but like i said I've had issues setting it up. So a bit about what i'm trying to do: l am using a 1756-L74 CPU with a 1756-EN2T, these are capable of being set up for open socket communications. I am also testing the communications on an S7-1200. I have both on the network and they run fine independently Issues: I have set up the software in the Allen Bradley software and set it as the server, however i am not sure what port i should set up on this? In the TIA software, I have set it up to act as a client but i am not sure what the Connection ID or Communications port should be? I get 16#809B as a ConStatus & 16#80A3 as a DisConnStatus Any ideas or experience with communications between bradley & siemens would be appreciated. Thanks, Ash |
| 10/23/2017 5:41 PM | |
|
Joined: 7/7/2010 Last visit: 12/18/2025 Posts: 16318 Rating:
|
Pretty sure you can just install the T_COMM library to your s7-1200. Nothing seems to be specific to the s7-1500. Download the project library, upgrade to your version of portal, refer to the documentation and see if it works. I think it will save a lot of time. That library is not know-how protected, so you can open the scl source and look at it.
|
|
science guy |
|
This contribution was helpful to
|
|
| 12/3/2019 8:16 AM | |
|
Posts: 4 Rating:
|
I am facing the very same problem. PLC are not connected by this process. let me know how you made connection. please post your screen shot. |
| 3/14/2024 11:01 PM | |
|
Joined: 9/21/2021 Last visit: 6/12/2025 Posts: 1 Rating:
|
Same issue, but not able to communicate even by switching the SIEMENS & AB PLCs between being the server or client. |
| 6/17/2024 7:40 AM | |
|
Joined: 3/21/2023 Last visit: 10/14/2025 Posts: 15 Rating:
|
Hello , Where can I download the T_COMM Library from? , So I can add it to my code. Thanks in Advance, |
Follow us on