4/12/2019 6:25 PM | |
Posts: 7 Rating: (0) |
Hello! I been tried an iot2040 for a small project. I followed all the steps of the Starter Guide and WIFI_USB.pdf tutorial, connecting with PUTTY, and then programming the iot2040 doing exactly the same as in the tutorial, but when I plug in the wifi dongle (PI official WLU6331) and type the command: /etc/init.d/networking restart I have this error: root@iot2000:/etc# /etc/init.d/networking restart Running /etc/init.d/networking restart is deprecated because it may not enable again some interfaces Reconfiguring network interfaces... ifdown: interface wlan0 not configured udhcpc (v1.24.1) started Sending discover... Sending discover... Sending discover... No lease, forking to background Successfully initialized wpa_supplicant Could not read interface wlan0 flags: No such device WEXT: Could not set interface 'wlan0' UP wlan0: Failed to initialize driver interface ifconfig: SIOCGIFFLAGS: No such device root@iot2000:/etc# nano wpa_supplicant.conf What can i do? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 4/15/2019 7:47:12 AMNew subject after splitting |
|
Follow us on