Industry Online Support
Technical Forum
6/7/2019 1:31 PM | |
Joined: 9/30/2016 Last visit: 8/15/2024 Posts: 914 Rating: (6) |
Please also see the attached screenshots. I am installing an Engineering Station (with some older versions of the Siemens SW to match the machines that are still using these version) and I have recieved a pic from a vendors Engineering Station - which should be working with the machines. I am unfortunately getting a warning / error error that some of my sw is either too old or not installed (and some of the remote I/O nodes are missing when I open the HW Config). What the screenshots show is that a working ES has S7-PCT V3.3 (HF2) installed but my new (not working) ES only has S7-PCT V3.2 installed - as far as I can see that is the only thing than can be too old. IS the error due to the slightly too old S7-PCT or the errors due to something else (and if so what)? S7-PCT V3.2 IS the version contained in the S7 SR4 DVD used. Which DVD can I find S7-PCT V3.3 (HF2) on? Would it work (without any migration problems) if I simply install S7-PCT v3.5 SP1 as I have that version on a DVD - or S7-PCT v3.5 Upd. 1? AttachmentAES'er.zip (47 Downloads) |
Last edited by: xmnj at: 06/07/2019 13:34:44Attachment |
|
6/11/2019 7:32 AM | |
Joined: 8/21/2014 Last visit: 9/25/2024 Posts: 1024 Rating: (14) |
Closed because the question was already posted here: How do I install S7-PCT The Helping Hand |
My Forum is the place to personalize your profile, |
|
Follow us on