1/20/2020 9:53 AM | |
Joined: 1/6/2019 Last visit: 8/27/2022 Posts: 13 Rating: (0) |
i am working with PCS7 V8.2 : step 7 v5.5 + SP4+HF9 / Wincc V7.4 my project contains : 1 ES + 2 OS Server ( Redundant servers) + 3 OS clients : ES HW : wincc appl + cp1623 ( 1) ( 170.10.1.83) + cp1623(2) ( 170.10.2.83) + IE general ( 170.20.1.10) SERV 1 : wincc appl + cp1623 ( 1) ( 170.10.1.81) + cp1623(2) ( 170.10.2.81) + IE general ( 170.20.1.11) Note : -each CP 1623 have two configured adress in siemens communication settings, i am using ip adress industrial ethernet in my HW configuration in step7, and not the NDIS. is this right? - ES1 OS : windows 7 édition intégrale - SERV1 OS : windows server 2012 R2 - i am using siemens PC stations. i have several problems: 1- i can't open wincc in ES1, wincc explorer display error message " server not available", i can't even create a new local project ( same error message) 2- in windows explorer networks --> i can't acces to any component of the network, even shared folder of ES1 are not accesibles from ES1 and an error message is displayed : windows can't access to \\ SERV1 or to \\ ES1 \ folder 3 - when i ping PCs everything is ok , when i configure SERV1 from Engineering station (ES1), configuration is succesfully completed , but when i want to download server HW form ES1 to SERV1 i have an error message " module IE GENERLA ( index 4 ) in station SERV1 cannot be started). 4 - in simatic shell i can see all Pcs and projects in them , but status of serv1 and ES1 is showing ' station up ' and i can't enter to any project. i am looking for urgent help please and what should i do to ensure communication between all network components. Attachmentscreenshots.zip (50 Downloads) |
Follow us on