1/13/2010 10:41 PM | |
Joined: 10/7/2005 Last visit: 5/14/2024 Posts: 3005 Rating: (1048) |
Hello Tomy Master WinCC Flexible 2008 Advanced (6AV6613-0AA51-3CA5) is the Engineering Software which "merely" allows you to configure/engineer yourWinCC Flexible application for a PC. To be able to "run" your application on a PC you willneed to additionally buy WinCC Flexible 2008 AdvancedRuntimewhich is a tag based license and available as followed: 128 tags: 6AV6 613-1BA51-3CA0 512tags: 6AV6 613-1DA51-3CA0 2048tags: 6AV6 613-1FA51-3CA0 4096tags: 6AV6 613-1GA51-3CA0 Please note that you will need to buy one Runtime license per PC on which you want to "run" you application will forever and a day allow you to "engineer" as many WinCC flexible application as you wish. I hope this helps |
Cheers |
|
1/14/2010 10:57 AM | |
Joined: 10/7/2005 Last visit: 5/14/2024 Posts: 3005 Rating: (1048) |
Hello again Tomy Master I think I know where the confusion comes from. You are in principal correct,WinCC flex Advanced Engineering software (6AV6613-0AA51-3CA5) does come with a "RUN TIME". It actually comes with two runtimes, one is the Simulation runtimewhich allows you to test/simulate your configuration and the other is the"real" runtime. While you can use the latter to also test your configuration (and for that matter in conjunction with PLCSIM if you wish), it will "complain" ifthe appropiate tag count related runtime license is NOT found. Bottom line is as before: If you want to have your WinCC flex Advanced engineered application run "permanently" on a PC you will need to buy one of thepreviously listed Runtime licenses. I hope this helps |
Cheers |
|
Follow us on