6/25/2013 11:29 AM | |
Posts: 3037 Rating: (192)
|
Hello, You can see which cable do can use for downloading to IPC. See in the list PC systems: http://support.automation.siemens.com/WW/view/en/19109408 http://support.automation.siemens.com/WW/view/en/58522603 http://support.automation.siemens.com/WW/view/en/29054992 Tweety |
6/25/2013 1:35 PM | |
Posts: 3037 Rating: (192)
|
Hello, Yes you can use download via file option. online > extended download to device > PG/PC interface "file system". You can start the project via douple clickon the file "pdata.fwc". Or you use the rt loader. It is the same as WinCC flexible. "pdata.fwx" is "pdata.fwc" Manuelles kopieren der Runtime Datei "*.fwx" auf den Visualisierungs-PC http://support.automation.siemens.com/WW/view/en/29054992 Tweety |
6/26/2013 5:42 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
Dear Tweety, today i went to site. the situation is diferent. 1. IPC 677c used. 2. Wincc runtime proffessional v11 sp2 update2 is installed. 3. In engineering laptop, wincc proffessional v11 sp2 is installed. 4. Established the communication between laptop and IPC, given all permission.(for testing purpose copied pdf file to IPC from laptop via network, which means no problem in security,sharing,permission etc) 5. Via download file-> browse the destination(IPC shared drive's folder) and selected load option. 6.System started the transferring. 7. In between error came "download failed" . no other description why it failed. no entry in log file of pjct backup. 8. checked the destination folder, found many folders, most of them are empty. 9. there was no .MCX file which is applicable in the case of wincc proffessional. 10. tried the same thing by configuring Wincc Rntime Advance , everything is fine. .FWC file is created at destination, working fine. 11. Because of this problem, installed wincc prof development software in to IPC, copied the pjct to ipc via pendrive and activated start run time. found ok. This option given for temporory purpose Please see the attached file. download procedure followed, file copied to destination folder screen shot are attached. please give solution regards vipz Attachmentforum.zip (361 Downloads) |
|
|
7/3/2013 11:56 AM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
nobody is came across this problem ?? |
|
|
7/7/2013 5:36 PM | |
Joined: 9/2/2012 Last visit: 4/18/2024 Posts: 711 Rating: (30) |
settings i made are attached. regards vipz Attachmentforum.pdf (507 Downloads) |
|
|
This contribution was helpful to3 thankful Users |
2/24/2014 11:49 AM | |
Posts: 101 Rating: (6) |
Thanks for this. But it has to be same user on both PCs? How practical. |
Follow us on