Industry Online Support
Technical Forum
2/14/2012 11:53 AM | |
Posts: 836 Rating: (100)
|
Hi, recently I found a FAQ regarding diagnostic of redundancy state of CPU without asset management / maintenance station. For the moment it is only available in german and spanish language, but I think the english translation will follow soon. Maybe it gives you some ideas: http://support.automation.siemens.com/WW/view/de/57119846 Furthermore there are several options for diagnostics without asset management: - You can use WinCC Lifebeat Monitoring to supervice the connection state to AS Stations and more. You can find informations in the WinCC help. - You can use PCS 7 Basic diagnostic where are no licences are needed. Right click on a plant hierarchy folder "Plant Hierarchy > Settings...". Check out the Help button in this dialog, there the basic diagnostics is descriped. If this is not enough, you can project a full diagnostic by yourself, but then you have to do everything what asset management is doing by your own. This might be a little bit of work. You also can project full diagnostic and analyze the objects / scripts in the WinCC pictures and then do it manually. |
Follow us on