Industry Online Support
Technical Forum
7/13/2011 2:01 PM | |
Joined: 10/7/2005 Last visit: 9/20/2024 Posts: 3021 Rating: (1054)
|
Hello jun-jun did you do a search at https://support.automation.siemens.comfor "Y-link"? If so I'm not too sure why it didn't yield enough information, but below are a few selected links which will hopefully help (and not contain too much "litter"): Manual: Bus links DP/PA coupler, DP/PA link and Y link FAQ's: How is the Y link structured? Which active backplane bus modules do you need when using the DP/PA link or Y-link? Configuring an S7 CPU as DP slave on the H system using a Y-Link P.S: You'll also find plenty of Forum related discussions with the same search, use the "Search area" buttons at the top of the screen to filtersearch results. |
Last edited by: fritz at: 7/13/2011 2:10 PMLast edited by: fritz at: 7/13/2011 2:06 PMadded links again (forum is playing up ...) Cheers |
|
Follow us on