Industry Online Support
Technical Forum
11/26/2014 11:18 AM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||
Posts: 204 Rating: (29) |
Hi, Taking the following example you can setup a simple MODBUS master-slave communication between s7-200 SMART and Sinamics v20. Note:Find the Sample Program in the attachment. Requirement: To operate the MODBUS protocol you must first procure and install first the STEP7Micro/WINSMART Parameter matching For MODBUS communication, on the master side you need library blocks "MBUS_CTRL" and "MBUS_MSG" MBUS_MSG
MASTER MBUS_CTRL
AttachmentMODBUS V20.zip (2618 Downloads) |
||||||||||||||||||||||||||||||||||||||||||||||||||||||
This contribution was helpful to4 thankful Users |
Follow us on