11/24/2006 10:36 AM | |
Posts: 14 Rating: (1) |
Hi, I have 10 internal tags with 5 sec logging cycle/ mode - cyclicand Data Logs, which is stored on a disk like a file, with 10 entries. That's very simply project. Look at attached files(prt sc). I want to have a log file,which is updated every 5 sec,with 10 lines. That's all. BUT instead of that i've got the log file with 9 lines only and in addition there are 8 tags recorded.(look at the attached file). That'sreally strange, isn't that ? If i setup up 10 entries for Data logs, i expect 10 tags record. I think that way it shloud work and maybe that's my opinion only. Thankseveryone for reply. AttachmentArchive.zip (137 Downloads) |
11/28/2006 7:32 PM | |
Posts: 3149 Rating: (171)
|
Hi, could you please attach a small testproject in the Forum or send it to the forum-moderation??? nemo |
11/29/2006 3:20 PM | |
Posts: 14 Rating: (1) |
Hi Thanks. But that's not working likeyou wrote. I did modification(12: number of data records per log)and checked my .csv file.I have to say that's was very funny. The numbers of logged tags has been chaning from 9 to 11 cyclic when RT ran. Check attached files. Attachmentlogged_tags.zip (111 Downloads) |
2/23/2018 4:01 PM | ||
Joined: 2/5/2013 Last visit: 3/26/2024 Posts: 287 Rating: (5) |
Nowdays with a TP1500 same random data is shown:
Is there a solution for Tia V14 sp1 update 2 and the TP1500? |
|
Follow us on