7/14/2016 9:04 PM | |
Posts: 2 Rating: (0) |
Hello I need more information about VSM10. I was searching information about "Bypass function" using a Sinamics G130. This Sinamics G130 starts two loads, one is a steel mil (I=487A) and other a fan (I=395A). In a specific situation I will transfer one load to line supply and Siemens shows some possibilities using VSM or not. I have to connect line supply in the terminal X522 or I have to connect this terminal X522 in the load side. I wrote it because I found two information in operating instruction manual, so I´m lost. See attachment. I need more information about reactor used to de-couple the drive converter from the line supply. We have two options to use this reactor, one I use with degree of overlapping and one I use without degree of overlapping. Where do I find more information? See attachment. Best reguards! ------------------------------------------------------------------------------------------ AttachmentExample.pdf (355 Downloads) |
Last edited by: Min_Moderator at: 7/15/2016 12:40:56 PMNew subject after splitting |
|
Follow us on