1/13/2016 12:15 AM | |
Posts: 14 Rating: (0) |
Hi, I have to transfer the inputs & outputs to an DB. The probleme comes when I try to LOAD bit by bit (LIST language) , TIA Portal said thats is not possible cause (textually): "The bit is not authorised for this instruction" (see picture). Why in CONT langage works? (see picture) Do you have any methode more easy or performance to put all my inputs and outputs directly in my DB (in the good address)?. My supervision HMI has to conect with the DB. ------------------------------------------------------------------------------------------ Attachmentphotos.zip (513 Downloads) |
Last edited by: Min_Moderator at: 1/13/2016 9:40:04 AMNew subject after splitting |
|
1/13/2016 10:39 AM | |
Posts: 14 Rating: (0) |
Hi, Thanks for you answer, but the problem is still there. I did the first solution and no problems (see photo 1). The problem is that I have many Inputs & Outputs (digitals & Analogics) , so that is a lot of work to write bit by bit. The second solution seems more performant but I have only BITS (not double words). Attachmentphoto.zip (512 Downloads) |
1/14/2016 5:16 PM | |
Posts: 14 Rating: (0) |
Thanks again, Very hepfull your suggests... When I put my FB Inside of OB1, do I have to fill the FB1 with all my inputs???. It's not enough to just load the block? Thanks very much AttachmentScreenshots.zip (412 Downloads) |
Last edited by: ICOMR at: 1/14/2016 5:23:52 PM |
|
Follow us on