Industry Online Support
Technical Forum
7/3/2014 9:29 AM | |
Joined: 5/10/2006 Last visit: 3/14/2024 Posts: 19 Rating: (0) |
Dear All Expert and Memebers, I'm trying to use the blocks of the Burner application example for Distributed Safety and F-Systems in a S7-400FH and PCS 7 v8.0 (at the moment with PLCSIM), but I can not get them to work as described in the manual: all initial conditions and interlocks are ok and the chart F_IGNTR seems to work correctly: block valves are opened and the flame detected. At this point must be turned on the burner (F_GAS_BU chart): so the block valves are opened and the flame detected before the timer T_IGN expires, but when the timer T_IGN expires the block valves are closed while they should remain open unless you press the stop burner button push button. There is someone who has already had experience with these blocks, or who has any Step 7 example project for a BMS? Thank You and best regards Mauro |
7/31/2014 4:54 PM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi Mauro, have you solved your problem in the meantime? Regards jumo |
7/31/2014 6:33 PM | |
Joined: 5/10/2006 Last visit: 3/14/2024 Posts: 19 Rating: (0) |
Hi jumo, not yet... I'm in contact with Siemens Technical Support that is currently investigating this issue Regards Mauro |
8/1/2014 9:14 AM | |
Joined: 11/16/2012 Last visit: 3/22/2024 Posts: 227 Rating: (31) |
Hi Mauro, thanks for the information. Please post theresult, once you got an answerfrom Technical Support. Regards jumo |
Follow us on