9/17/2019 6:46 AM | |
Joined: 10/17/2007 Last visit: 10/9/2024 Posts: 4039 Rating: (354)
|
I think you already have basic ideas for 840D, so check Post in this forum--"840D encoder disable " you need set MD 30130=0 MD30240=0 and make drive "Not active " https://support.industry.siemens.com/tf/ww/en/posts/840d-encoder-disable/219538/?page=0&pageSize=10 |
If you like my comments please |
|
10/1/2019 6:53 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (877)
|
Hello, Post title states system is 840D SL & you mentioned servo motor type 1FT5. Please note, 1FT5 series servo motors are not compatible with Sinamics drives i.e. 840D SL. Please refer SINAMICS, SIMOTICS: 1FT5 Servo Motors with SINAMICS Drives FAQ for more information. I think it must be 840D PL (power line) Please check NCU box & provide NCU MLFB number which will clear confusion/doubt. Now if you want to check servo motor encoder, you need to activate motor encoder. To do so, set Y axis MD 30200 = 1, so external scale feed back will not be in system, retain all other parameters as it is. In axis service menu [Press Dianosis > SERVICE DISPLAY > SERVICE AXIS > select AXIS + or - KEY to select appropriate axis] check Y axis measurement system 1 is active i.e. GREEN LED must be ON, if it is not you need to check system PLC ladder logic & set logic so that DB3X.DBX1.5 = 1 (here X = 1 or 2 or 3. I hope in your case it must be 2) means motor encoder feedback system is enabled. Then you can move the axis & check. If it works without any alarm, it means motor encoder is OK. If it trigers any alarm, you may revert with alarm details. It is always better to attach snap shot of alarm which will help in diagnosis of fault. HTH |
Last edited by: The Helping Hand at: 10/01/2019 11:08:53Optimized link. |
|
This contribution was helpful to1 thankful Users |
10/1/2019 6:48 PM | |
Joined: 3/12/2015 Last visit: 10/8/2024 Posts: 534 Rating: (15) |
|
10/3/2019 11:36 AM | |
Joined: 3/12/2015 Last visit: 10/8/2024 Posts: 534 Rating: (15) |
Backup
AttachmentMach145.zip (364 Downloads) |
Follow us on