8/5/2021 6:53 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
another image |
8/5/2021 6:55 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
led status video
AttachmentWhatsApp Video 2021-08-05 at 9.38.00 AM.mov (525 Downloads) |
8/6/2021 5:15 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (873)
|
Hello, Welcome to forum. You can make a folder & insert video clips & images in it, compress the same folder & attach to your post, instead attaching separetly to individual post. Now to your query. from your description it looks like NCU battery is weak & due to frequent power failuers, PLC data seems to be lost. From the attached snaps, 7 segment displayed 6 which indicates NC booting is OK, but RED LED PS & PF indicates that PLC watchdog error has detected & PLC is in STOP mode. First you need to replace NCU battery so that this problem will not repeat & clear NC & PLC data. Please check if you have valid NC, PLC data either on your NC card (if you have PCU20 or PCU50 you can check it in Program Manager ->Archieve Folder --> NC.arc & PLC.arc files) or on externa; storage device like PC. Please refer attached sheet which will help you to understand NC, PLC data clearing & restoring procedure. HTH Attachment840d PL NC___PLC_Data_Clear & restore procedure.pdf (664 Downloads) |
Last edited by: PISCEAN 2010 at: 08/06/2021 05:19:17 |
|
8/6/2021 7:45 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Thanks a lot for your help. We have all this files .ARC in the ARC folder. Wich files needs to restore? Best regards Diego C Attachmentarc.dir.zip (481 Downloads) |
8/13/2021 10:23 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Ok, I will try with those files. best regards Diego C |
8/23/2021 7:08 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Hello, After explore the content of the information inside the Hard Disk and send you the files that has the newer backup, I made a Clone of the Disk beacuse the original mecanical disk make a noise inside the disk. After that I placed the disk again in the machine, but this time the system wont boot. The screens are in the information in the attached pictures. I will wait for your advice Best regards
Attachmentpictures840D-v1.zip (542 Downloads) |
8/27/2021 11:08 PM | |
Joined: 7/29/2021 Last visit: 6/8/2023 Posts: 9 Rating: (0) |
Hello, both disk, the clone and the original give us the same screen, wont boot. Is There any way to recover the data? |
Follow us on