12/15/2016 3:20 PM | |
Posts: 2 Rating:
|
Nevermind, I had the feed knob on the simulator control at 0 . |
4/2/2019 11:54 PM | |
Posts: 5 Rating:
|
Hi, I have the same issue. I have checked the MD mentioned above and it is 0H. The feedrate knob is also not at 0%. However, when I try to jog the axis, I get the Wait: axis enable missing error. I get the same error if I try to execute a program. The simulation runs, but not the execution. Axis show as referenced if I check under the 'Ref Point' screen. Please let me know if anyone knows how to enable the axes. I am running Sinutrain 4.8 SP4 on Win 10 64 bit with the DEMO-Lathe machine and the basic license. Thanks! |
Follow us on