7/16/2018 1:25 PM | |
Posts: 531 Rating: (34) |
Could you tell us what the error tells you? We need more information to help! |
7/16/2018 3:49 PM | |
Joined: 3/24/2009 Last visit: 8/7/2023 Posts: 406 Rating: (3) |
Hi, If you are using Windows 10 or Windows server 2012 OS then you have to do this. Source files for .Net framework 3.5 feature are not installed as part of typical installation. Please refer the attachment, it works for me. Hopefully it will help AttachmentSolution.pdf (1404 Downloads) |
All is well :-) |
|
7/17/2018 6:42 PM | |
Joined: 10/7/2016 Last visit: 5/22/2024 Posts: 66 Rating: (1) |
Hi samkcr, I already try it but do not works, I already make Iso download from microsoft site and don't work |
1/2/2019 3:55 PM | |
Joined: 10/18/2012 Last visit: 8/21/2024 Posts: 225 Rating: (23) |
Dear Gustavo Dias, for Windows-10 Embedded LTSB 2016 for Windows Server 2016 All required steps to install .NET Framework 3.5 are documented here: best regards, |
Follow us on