4/22/2019 10:45 AM | |
Joined: 3/9/2012 Last visit: 8/10/2024 Posts: 236 Rating: (0) |
What exactly you want to do? |
4/22/2019 11:41 AM | |
Joined: 9/19/2009 Last visit: 9/21/2024 Posts: 459 Rating: (85) |
Hi HMIRuntime.Trace is your friend here... and you can use the sleep function to see what is happening, make visible the object and debug it. Also, You can check if the file is open , before create the Excel Object Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/22/2019 12:51 PM | |
Joined: 9/19/2009 Last visit: 9/21/2024 Posts: 459 Rating: (85) |
Hi Sorry, I can´t reproduce your behaviour , for my works fine, the procedure and the action every 10 seconds I have create a new procedure WriteExcel and I call this procedure from the button and I call the same procedure in my cicly action every X time. See PM. Regards |
If my answer help you, use the Thanks or Rate Button, It is free of charge :-) |
|
4/29/2019 12:54 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (41)
|
Hi, which version of Excel and WinCC do you use? Hopefully they are compatible and have been installed in the correct order (First Office then WinCC). B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on