4/1/2015 1:11 PM | |
Posts: 12 Rating:
|
Hello,
---------------------------------------------------------------------------------------------------- |
Last edited by: Min_Moderator at: 4/1/2015 4:26:33 PMNew subject after splitting |
|
4/1/2015 5:03 PM | |
Joined: 1/5/2011 Last visit: 3/13/2025 Posts: 815 Rating:
|
Hi dlk, most easy solution is to use the any pointer to disassemble the DATE_AND_TIME. Check out the attachment for an example. Check out following link if you have problems implementing the AT keyword: FAQ How do you program the overlapping of tags with the keyword 'AT' in the TIA Portal V11? Description With the "AT" keyword you can overlap a declared tag with another declaration if, for example, you want to access the separate bits of a tag of the Word data type with an Array of Bool.... You need the following to overlap tags with the keyword "AT".... In the drop-down menu you select the keyword "AT" and then click in the "Name" column.... The separate input tags of the Bool data type are assigned to For products: 6ES7513-1AL00-0AB0, 6ES7211-1HD30-0XB0,...All products
Kind regards, |
Keep it simple and on-topic. |
|
This contribution was helpful to
4 thankful Users |
Follow us on