9/17/2014 4:06 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Look atthis page, chapter about features: Flexible use because slots are upwards-compatible, that is, no matter what slot is available (e.g. x4, x8, etc.), the CP will fit. Also, page 9 ofthis manualspecifies the same: Hardware requirements The CP 1623 requires a PCIe slot (PCI express x1; can also be operated in x4, x8 or x16 slots). BR, olloy
|
9/17/2014 5:11 PM | |
Joined: 3/20/2012 Last visit: 8/13/2024 Posts: 118 Rating: (1) |
Thanks a lot OLLOY. Best regards. |
3/2/2015 2:18 PM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! How exactly you decide it is not working? Driver persists in the system? |
3/10/2015 9:37 AM | |
Joined: 8/27/2010 Last visit: 4/13/2024 Posts: 417 Rating: (37) |
Hi! Please see this manual and specially chapter 3.1 and forward for details of instaling CP1623. |
11/30/2015 1:39 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4767 Rating: (123) |
New question published by rez@ is split to a separate thread with the subject cp1623(1):an internal error occurred. Best regards |
Follow us on