11/8/2018 3:44 PM | |
Posts: 11 Rating: (0) |
Hello. Does anyone have any experience running LXC containers in IOT2000? I successfully created a container with lxc-create but when I try to start the container with lxc-start I get this error message:
Any idea how to solve this? Thanks in advance. PS: I created a custom image with master branch of meta-iot2000 and rocko branch of meta-virtualization. I used this github repo I created. |
11/12/2018 1:46 PM | |
Joined: 4/28/2015 Last visit: 4/21/2024 Posts: 578 Rating: (43) |
The default kernel config of meta-iot2000 is missing some features needed for containers. Likely this commit will help in your case as well. |
This contribution was helpful to1 thankful Users |
11/20/2018 4:00 PM | |
Joined: 12/12/2016 Last visit: 4/8/2024 Posts: 640 Rating: (60)
|
Hello, Do you have an internet connection? Because the commit you are unable to fetch is online: add dragonfly bsd to the build tags Kind regards! |
11/22/2018 4:11 PM | |
Posts: 11 Rating: (0) |
Is it possible to have some guidance how to create a working image with lxc? I use this repository and I build my images using a docker container using the commits that were suggested above but LXC still doesn't seem to work. Thanks in advance. |
Last edited by: tsitsikas96 at: 11/22/2018 4:11:46 PMLast edited by: tsitsikas96 at: 11/22/2018 4:12:17 PM |
|
11/23/2018 4:58 PM | |
Posts: 11 Rating: (0) |
Hello, Yes I still get the same error. I am using the commits that are used in jan/docker branch. Shall I use morty branch instead of rocko? Thanks again. |
Follow us on