10/12/2010 9:02 AM | |
Joined: 10/7/2005 Last visit: 5/13/2024 Posts: 3005 Rating: (1048)
|
Hello ustcwangxx I must admit, this one is a bit strange. You are correct though,memory address 0002 3180(hex) is NOT directly explained in the 945 CPU manual and the reason for it is that this address space belongs to the operating system who's contents/structure is (most likely) only know bySiemens(see attached pic). As suchIdon't have the faintest ideawhat is contained in that address but wonder if there is a chance that the address 0002 3180(hex) as well asthe other 0002 31FE(hex) one in your S5 example logic is atyping mistake? If it isn't, I'd suggest to launch aSupport Request with Siemens, butperhaps other users here may know it too and care to share. I hope this helps and good luck |
Cheers |
|
Follow us on