11/19/2018 1:47 PM | |
Posts: 69 Rating: (0) |
Hello all of you dears , please i need answer for my question urgently , because i did a mistake but it's not on purpose . my question is i have automate step 5 115U cpu 942 and i have wih it the ram 6es5 375-old11 . the problem is i did overall reset then i remove the battery .so, i lost the program in the ram . fortunately, i had program on m PC and i transfer it o step5 but the problem i need to transfer it at the ram how could i do it ? please could you give step by step ? Best regards. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 11/19/2018 2:56:11 PMNew subject after splitting |
|
11/19/2018 3:52 PM | |
Joined: 5/6/2010 Last visit: 5/5/2024 Posts: 1965 Rating: (273) |
Hello, you should do the follow:
Then should it work. Please look at this S5-115U manual. Hope this is helpful regards |
Follow us on