4/22/2008 10:16 AM | |
Posts: 9 Rating:
|
Hello, I have the same problem. Does anybody have a solution? Thanks in advance Nicolas |
Last edited by: nicwincc at: 4/22/2008 10:18 AM |
|
4/22/2008 11:43 PM | |
Posts: 2661 Rating:
|
As far as I know this is not possible. The reason is, for any message type (in a message class), only 3 color settings can be done: - Came in - Went out - Acknowledged See attachment. That is why for Went out acknowledged also you are seeing steady red (like Came in acknowledged). Regards AttachmentDokument1.pdf (419 Downloads) |
4/23/2008 10:27 AM | |
Posts: 1084 Rating:
|
I have to agree with phantom. three message states and 1 message requesting acknowledgement (info/event). with regards, Ikkezelf |
4/28/2008 8:54 PM | |
Posts: 510 Rating:
|
The message status can be used to determine Came In, Went Out and Acknowledged Status. Consult the Online Help |
4/29/2008 4:41 AM | |
Posts: 2661 Rating:
|
That’s right. |
4/29/2008 6:45 PM | |
Posts: 2661 Rating:
|
I do not know if you can combine came in & acknowledged or went out & acknowledged in one status. But you can configure your alarm list to be able to see all three states. Double click on the WinCC Alarm Control and in the Message Blocks tab, check Status and Acknowledged. See attachment. Hope this is helpful. AttachmentDokument1.pdf (362 Downloads) |
Follow us on