3/3/2020 2:53 AM | |
Joined: 4/3/2017 Last visit: 8/7/2025 Posts: 69 Rating:
|
Hi, i want to do virtual commissioning of SINAMICS V90 drive and servo motor 1FL6. Also I have Tia portal v15.1, plc-sim advanced. Basically, I want to control servo motor using TO (technology object) from TIA portal. Is it possible to just control shaft of servo motor in NX (I have 3D model of servo motor) with TO from TIA? Do i need SIMIT to configure SINAMICS drive and motor? How to simulate SINAMICS drive like it is real? I have read https://support.industry.siemens.com/cs/ww/en/view/109760078 and there is written as a feature : "Use of simulated axes without drive simulation ". And here: https://support.industry.siemens.com/cs/document/109754823 "Use of real axes (not simulated) " and "Drive simulation via PROFIdrive telegram 105". How can I do drive simulation and use NX MCD to see shaft rotating? Best regards, LF |
4/27/2020 7:21 PM | |
Joined: 2/25/2014 Last visit: 6/29/2025 Posts: 61 Rating:
|
You have to add GSD file of SINAMICS drive with telegram to Technology object(TO), speed, position axis. it will be hardware connection in the virtual between GSD files and SIMIT Profidrive 2(made telegram 102 or 105), sinamics and Sensor. So, you can be done simulation after that working hardware concept in the virtual. |
4/29/2020 11:05 AM | |
Posts: 37 Rating:
|
Hi, for a holistic simulation or virtual commissioning we recommend using SIMIT (https://support.industry.siemens.com/cs/us/en/view/109758943) For easy simulation you can set your Technology Object to simulation mode. bg, |
Last edited by: Jen_Moderator at: 04/29/2020 13:36:29Optimized link. |
|
Follow us on