(2)| 5/13/2020 12:32 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, Since you have created subprojects inside your multiproject (which is good), you must merge all separate projects together to create one plant bus. In order to do so, execute the following: 1. Go to Plant View and right click the multiproject 2. Select Multiproject->Adjust Projects 3. Select: Ethernet from the list under Merge/DownSubnets and press button: Execute. The subproject Ethernet connections are now merged to form one Ethernet net. Now, you can assign the ES to AS and do further project modifications. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/13/2020 1:21 PM | |
|
Joined: 3/14/2008 Last visit: 1/15/2026 Posts: 2233 Rating:
|
Hi, For each subproject: Project AS, Project OS, Project ES etc. you create a local plant bus. Call them whatever you like, for example: Subproject AS: Plantbus_AS, subproject ES: Plantbus_ES etc. After you are done, then merge all subnets into Ethernet Wide. Now you can make connections from AS to ES for example. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/13/2020 1:56 PM | |
|
Joined: 11/24/2016 Last visit: 4/25/2024 Posts: 99 Rating:
|
Thankyou Oreca for your help and support. I appreciate it. |
Follow us on