5/14/2017 2:11 PM | |
Joined: 2/8/2017 Last visit: 3/15/2024 Posts: 87 Rating:
|
Dear all, just share my "Library for Nokia Graphic Display LCD4884 LCD - SPI" :-) The library is based on the example from DF Robot as Arduino Shield I just to the rework to fit the library to fit everything to the IOT2000 and indroduce some more functions like the "virtual display" PLEASE take note: The pin mapping dosen't fit to the native SPI, but the library use the nativeinterface! Any hinds are welcome. Regards AttachmentNokiaDisplay_SPI_LCD4884.zip (1058 Downloads) |
This contribution was helpful to
1 thankful Users |
Follow us on