3/4/2020 9:02 AM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating:
|
I've followed up on that ticket on github, let's see... |
3/4/2020 4:27 PM | |
Joined: 4/28/2015 Last visit: 6/28/2024 Posts: 578 Rating:
|
Information coming in piecewise: According to https://github.com/Cloud-Automation/node-modbus/issues/236#issuecomment-594553174, the issue is also solved in node-red-contrib-modus 5.x. So, triggering an update via the palette should help as well (and is likely easier). |
This contribution was helpful to
1 thankful Users |
3/4/2020 8:03 PM | |
Joined: 4/11/2013 Last visit: 5/22/2024 Posts: 56 Rating:
|
Hi jan-k, I will try this. I thought it was ok with version 5.x but this wasn't the case. I will make a fresh image and test several suggestions. René |
Last edited by: joshuatreenl at: 03/04/2020 20:30:02 |
|
3/4/2020 9:47 PM | |
Joined: 4/11/2013 Last visit: 5/22/2024 Posts: 56 Rating:
|
Hi Jan 1. Fresh image v2.6.0 (node-red-contrib-modbus version 4.1.3). Result: node-red logfile increase very fast -> messages Modbus Server 2. Modification as described (line 251, file modbus-server-response-handler.js). Result: no messages (Modbus Server) in node-red logfile. 3. Set version 0.0.6 (file: node-red-node-intel-gpio) *Don't know if this is necessary* 4. Upgrade node-red-contrib-modbus version to version 5.2.0 (via node-red manage palette). Result: no messages (Modbus Server) in node-red logfile. Conclusion: 1. It seems that the problem (as mentioned above) is solved if an update is performed (node-red-contrib-modbus version 4.1.3 -> 5.x). 2. I don't know if this is important (check https://github.com/BiancoRoyal/node-red-contrib-modbus/blob/master/README.md) Based onmodbus-serialwith TCP, C701, Telnet, Serial, RTU buffered, and ASCII
Node-RED v0.x versions:
Node.JS 8.x is supported with v3.x and the version installed is v5.x... I'll hope this won't be a problem. 3. The logfile now contains another message (every minute): @Jan: Thanks for your help! René |
Last edited by: joshuatreenl at: 03/04/2020 22:06:57Last edited by: joshuatreenl at: 03/04/2020 22:08:08Last edited by: joshuatreenl at: 03/04/2020 22:48:00 |
|
This contribution was helpful to
1 thankful Users |
Follow us on