4/5/2020 2:32 PM | |
Joined: 11/6/2017 Last visit: 8/15/2025 Posts: 16 Rating:
|
Hi, I have a wincc v6.2 project. I migrated it to v7.0 first. Then, I migrated it from v7.0 to v7.2. When it was runtime, I press the buttons to pass between graphic pages. But following message is coming to the screen and runtime is deactivating; "Unhandled exception was raised.Look file"C:\Program Files(x86)\Siemens\WinCC\Diagnose\PDLRTSEH.LOG" for details. I added PDLRTSEH.LOG . What can problem happen? Thanks. AttachmentPDLRTSEH.zip (572 Downloads) |
4/6/2020 7:15 AM | |
Posts: 8 Rating:
|
Hello. You may have problems with the graphics driver. Try reinstalling it. |
12/2/2020 7:46 AM | |
Joined: 2/1/2019 Last visit: 9/19/2024 Posts: 21 Rating:
|
I also got this error message, but I did not touch the project before. Any idea why did it happen? |
12/2/2020 2:18 PM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello tiby007, this is caused by an access violation, which has happened If you would not such messages, you should use the SIMATIC Assessment Suite https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Service Request and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on