12/3/2013 3:43 PM | |
Posts: 30 Rating: (0) |
Hello everybody, I have a siwarex 7mh4950* with SF due to adc overload in channel 2 as i checked in siwatool. channel 1 works fine, i also calibrate channel 1 with no problem. I have disconected the three loadcells from the junction box because i thought that the problem was a defective loadcell and i reconnect them one by one but the SF and the adc overload is still there. Any ideas for the spesific error? I didn't measure the voltage between EXC+ to EXC- and SEN+ to SEN- yet. I also upload print screen with the problem. Thank you in advance Attachmentsiwa.zip (430 Downloads) |
Last edited by: Skaras at: 12/3/2013 4:04 PM |
|
12/6/2013 2:38 PM | |
Joined: 1/4/2007 Last visit: 9/2/2024 Posts: 1142 Rating: (175)
|
Hello Skaras, Well, the resistance of load cell 3is too little. Anyway I’m still interested in the voltages. Best regards Siwarexi |
12/6/2013 2:51 PM | |
Posts: 30 Rating: (0) |
Thank You, Because i am far away from the project i cannot measure the voltages. I suppose that the next week i'll be there so i will send you the voltages. |
Follow us on