12/15/2017 2:35 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating: (1051) |
hi Egatech, I found this application sample hope this helps, regards, |
FCK WAR! |
|
12/29/2017 11:25 AM | |
Posts: 2 Rating: (0) |
Apologies, I did not explain properly as I was looking at different solutions and got mixed up. I actually have now 4 linear motors with about 26 or 52 pulses/mm and the speed is controlled via PWM. The pulses will tell me the speed as some motors are opening or closing, as some motors are a bit faster than others when connected to the same pulse. I managed to do a speed control as so on, but my PWM is no sending out anything even though that all seems correct. My apologies for possibly some silly mistakes but this is my first experience with S7-1200 and TIA as unfortunately I took this job assuming the motors would run at same speed and only when they arrived I realised that was not the case. AttachmentPWM Visual.pdf (135 Downloads) |
Follow us on