4/18/2018 7:20 PM | |
Posts: 2826 Rating: (685) |
Hello. My license is only for Step7 BASIC. I am unable to read the project code given in the application example: (Suggestion was made by huggy_d1 in this post [4/13/2018 6:49 PM].) It would be real nice if someone could help me out and port it for an S7-1200. Or even a PDF print-out would be nice. Looking at the PDF in the application example I could reverse-engineer something. My notes are given in the attached picture. The "zero" characters in-between bothers me in making a generic setup. Help would be appreciated. Regards. |
Last edited by: #dP at: 4/18/2018 7:28:29 PM |
|
4/19/2018 4:56 PM | |
Joined: 7/7/2010 Last visit: 9/27/2024 Posts: 15239 Rating: (2420)
|
The FB was not know-how protected. Here it is in SCL:
|
science guy |
|
This contribution was helpful to5 thankful Users |
4/19/2018 5:01 PM | |
Joined: 7/7/2010 Last visit: 9/27/2024 Posts: 15239 Rating: (2420)
|
If you use the Siemens FB as written, it expects the output DB to be configured as follows:
|
science guy |
|
This contribution was helpful to2 thankful Users |
Follow us on